AOUT#.VALUE
Description
AOUT#.VALUE reads the analog output value.
Examples
Context
For more information see Analog Output.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | V |
Range | 0 to 10V |
Default Value | 0V |
Data Type | Float |
See Also | |
Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AOUT1.VALUE | 0x3800 | 0x1 | INT | 1000:1 | - | RO | True |
AOUT2.VALUE | 0x3801 | 0x1 | INT | 1000:1 | - | RO | True |